Southco Resource Center

We hope you find something interesting to read, watch and share.
Securing the Future: Multi-Point Latching Solutions for Global Energy Storage Systems
June 17, 2026
Securing the Future: Multi-Point Latching Solutions for Global Energy Storage Systems

This case study illustrates how Southco partnered with a global leader in renewable energy technology, to develop a customized multi-point latching system for energy storage. Rather than addressing the need, this collaboration targets industry-wide safety, reliability, and operational efficiency across the global energy storage sector. 

Facing increasingly strict safety requirements for energy storage equipment, Southco delivered a highly reliable, explosion proof and well sealed locking solution for energy storage cabinets. This solution was designed to meet rigorous industrial protection standards while ensuring long term stable operation in harsh outdoor environments. With Southco’s engineering support, the customer has significantly enhanced the safety and durability of its energy storage systems. The customized multi point latching system delivers physical protection, sealing against water and dust ingress, friendly operation, aligning with the stringent requirements of leading energy storage equipment manufacturer.

Southco F2 multi-point latching system for energy storageSouthco F2 multi-point latching system for energy storage

Large energy storage in a harsh environment 

Beyond meeting product-level requirements, this innovation has positioned the leading player as a safety pioneer in the global energy storage industry while establishing new benchmarks for structural protection and enclosure reliability, that accelerates adoption of safety standards across utility-scale energy storage systems worldwide.

Challenge

The global energy storage industry demands higher safety, robust protection and reliable sealing for outdoor containers. The strategic customer of Southco sought a high-performance locking solution to meet explosion proof, waterproof and anti deformation requirements under harsh environmental conditions.

Solution

Southco developed a customized F2 multi point latching system specifically engineered for large scale energy storage cabinets and heavy-duty doors. Designed to enhance explosion proof and industrial safety standards, stable protection for energy storage equipment.

Value

Southco’s innovative locking solution enhances product competitiveness, improves safety and efficiency, solidifies the industry leadership of the strategic customer, and supports the large scale deployment of global energy storage.

The Challenge

As global energy storage deployment continues to scale, the industry is facing universal technical challenges for outdoor containerized systems. Conventional single-point locks struggle to meet industrial criteria, lacking sufficient structural strength, explosion-proof capability and environmental sealing for harsh operating conditions. These shortcomings contribute to common industry pain points such as cabinet deformation, poor anti-pry performance, labor-intensive operation and limited manufacturing tolerance that conventional off-the-shelf hardware cannot address.

As an industry leader, the customer encountered the same bottlenecks during its global expansion. To overcome these industry challenges and meet stringent requirements for explosion-proof, waterproof and anti-deformation performance, the global leader collaborated with Southco to develop a customized engineered latching solution.

The Solution

Southco collaborated closely with the strategic customer to develop a bespoke F2 multi point latching system designed for energy storage enclosure protection. Engineered to solve the most critical safety and operational challenges in large scale energy storage systems, the latching solution delivers industry leading performance across dimensions:

  • Extreme Load Capacity for Explosion Protection

A top priority for the leading player, the F2 multi point latching system provides a 5000N single-point working load, delivering the robust structural strength required to safeguard cabinets in demanding environments.

  • Superior Sealing for Outdoor Durability

The system achieves a 12mm compression stroke, which exceeds the market standard of 5–6mm. Combined with IP66-rated protection, the solution ensures stable, long-term operation in harsh climates.

  • Industry-Leading Ergonomics

With a 1:13 mechanical advantage (compared to the 1:7 or 1:8 ratio of standard locks), the F2 multi point latching system enables smooth, one-handed operation of heavy-duty doors, significantly improving maintenance efficiency.

  • Best-in-Class Tolerance Adaptation

Southco’s team optimized the latch to support up to 6mm of deformation tolerance. This built-in flexibility compensates for door sag and sheet metal variations, maintaining consistent sealing throughout the product lifecycle.

Southco F2 multi-point latching system Southco F2 multi-point latching system

Implementation and Results

The journey from concept to production highlights Southco’s expertise in delivering robust, application-tailored access solutions. By integrating the customized F2 system into the customer’s energy storage containers, Southco has delivered measurable gains in safety, reliability, and optimized the total cost of ownership. The solution exceeds rigorous explosion-proof compliance requirements, its superior sealing and durability significantly cut down on unscheduled   maintenance in extreme outdoor conditions.
This collaboration optimizes lifecycle costs and scales utility energy storage by strengthening structures, simplifying operations, and extending equipment life. The project demonstrates how precision-engineered hardware solves industry challenges to fast-track renewable energy technology.

Powered by Amasty Magento 2 Blog Extension