As vehicles become quieter, more connected and increasingly autonomous, the interior cabin is evolving from a space designed for transportation into an environment designed around people. People are no longer travelling from one destination to another; they’re attending meetings inside their vehicles, consuming content, sharing meals, and simply making the most of their time spent in transit.
As these activities become part of the in-vehicle experience, every interaction within the cabin contributes to how its occupants perceive quality. Large displays, intelligent infotainment, premium seating, and integrated comfort features are becoming part of a more connected and personalized experience.
The challenge for automotive designers then is not just adding functionality, but delivering it in a way that feels intuitive, refined and effortless. Even a seemingly simple feature, such as a tray table, can play an important role in bringing that vision to life.
From functional accessory to user experience touchpoint
Traditionally viewed as a simple convenience feature, tray tables have taken on a broader role as vehicle interiors become more versatile. Occupants increasingly expect practical surfaces that support a variety of activities, supporting everything from mobile work and video conferencing to dining and entertainment.
Occupants may never see the engineering behind the vehicle, but they do experience it every time they interact with it. So, how a tray table deploys or how stable it feels during use, and how smoothly it returns to its stowed position all influence that level of quality. That’s why tray tables have evolved into an important touchpoint that helps to define the overall cabin experience.
Engineering the feeling of effortless quality
The best cabin experiences rarely feel sophisticated. To the occupant, a tray table simply opens smoothly, remains stable, and folds neatly away when it’s no longer needed.
But achieving this balance requires careful integration of motion control, positioning and structural support technologies. Tray table systems must withstand repeated use while maintaining smooth operation, positional stability and reliable performance under varying loads and environmental conditions.
Friction hinges and constant torque technologies can allow for that controlled movement, secure positioning, and consistent operation throughout the product’s lifecycle. These details matter. A tray table that feels unstable, difficult to position or prone to vibration can undermine perceptions of quality. Conversely, controlled motion, precise positioning and consistent tactile feedback reinforce the premium experience occupants increasingly expect.


Southco tray tables deliver 180 degree fold out motion
This balance between technical sophistication and intuitive use is now a defining characteristic of premium interior cabin design. Engineering these moments correctly helps ensure that functionality enhances, rather than detracts from, the overall cabin environment.
Designing for space, simplicity, and functionality
As occupant expectations increase, OEMs face growing pressure to incorporate additional functionality without compromising interior aesthetics or available space. Today’s vehicle interiors must accommodate a growing number of features, including connectivity solutions, charging capabilities, and personal storage options. At the same time, occupants expect clean surfaces, uncluttered surroundings, and on demand functionality that does not dominate cabin space.
This presents a key design challenge: how can manufacturers add capabilities while preserving that openness?
Integrated, fold-away tray tables help manufacturers better balance these competing demands by providing useful functionality, while preserving clean, minimalist interior designs. When thoughtfully engineered to fit discreetly into armrests, seatbacks, or center consoles, they can remain unobtrusive when not in use, yet quickly transform the available space into a practical surface when needed.
These details may appear small in isolation, but together allow designers to maximize utility without sacrificing visual appeal or passenger comfort.


Seat back stowable tray tables reduce cabin space footprint
Designing for how people use their time
As automated driving technologies continue to evolve, the relationship between people and vehicles will change dramatically. Whether travelling in today's premium vehicles or tomorrow’s increasingly automated mobility platforms, occupants are already using journey time differently.
As a result, manufacturers are designing cabins around activities, not just transportation. Adaptive physical elements, including tray tables, work surfaces, comfort systems, and positioning technologies, will be essential to creating flexible, multifunctional spaces.
For automotive manufacturers, the opportunity lies in designing interiors that support how people want to spend their time, not just how they travel. And the features that support these experiences will play a deciding role in shaping how occupants evaluate comfort, usability and overall vehicle quality.
Creating better experiences through engineering
Creating memorable cabin experiences demands careful attention to the moments where people physically interact with the vehicle.
Drawing on decades of expertise in motion control, access hardware, and positioning technology, Southco helps OEMs and manufacturers engineer these critical touchpoints. From deployable tray table mechanisms and adjustable work surfaces to controlled-motion applications throughout the cabin, Southco solutions help manufacturers deliver functionality without compromising comfort, reliability or design freedom.
Discover the positioning, motion control and access hardware solutions helping OEMs deliver the next generation of occupant experiences:


Interaction in Future Fully Autonomous Cockpits